What shall be the power consumption of the core of MPC8379E (667Mhz) processor typically and maximum?. To design the 1.0V regulator for core supply.
Have a great day,
The estimated typical power dissipation for the chip device is shown in Table 5. Power Dissipation of the MPC8379E PowerQUICC II Pro Processor Hardware Specifications, Rev. 10. You can download it from the Freescale page
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MPC8379E
For core frequency 667MHz and CSB/DDR frequency 333MHz Typical is 2.1W (T=65’C) and Maximal is 4.1W (T=125’C)
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------