Hi,
I am trying to download android-5.0.2_r1 for SabreSD board.
I am following the steps as described in "Quick User Guide" document.
Everything is fine until the RED colored line:
$ cd ~
$ mkdir myandroid
$ mkdir bin
$ cd myandroid
$ curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
$ chmod a+x ~/bin/repo
$ ~/bin/repo init -u https://android.googlesource.com/platform/manifest -b android-5.0.2_r1
$ ~/bin/repo sync
$ cd ~/myandroid/prebuilts/gcc/linux-x86/arm
$ git clone https://android.googlesource.com/platform/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6
$ cd arm-eabi-4.6
$ git checkout android-4.4.3_r1
$ cd myandroid
$ git clone git://git.freescale.com/imx/linux-2.6-imx.git kernel_imx # the kernel repo is
large. Therefore, this process can take a while.
$ cd kernel_imx
$ git checkout l5.0.0_1.0.0-ga
After this red colored last command, I cannot continue and I get an error:
HEAD is now at 4f0dd92... Don't set console cflag to zero.
What can be the reason of the problem?
How can I solve this and proceed?
Best regards.
What's problem with "HEAD is now at 4f0dd92... Don't set console cflag to zero."?
It says "HEAD is now at 4f0dd92" and has a comment "Don't set console cflag to zero" when the engineer check in the code.
The is what I check out l_imx_3.14.28_1.0.0_ga
git checkout rel_imx_3.14.28_1.0.0_ga
HEAD is now at 91cf351... MLK-10439: arm: imx: fix system hang after resume back under low busfreq
"MLK-10439: arm: imx: fix system hang after resume back under low busfreq" is what the engineer checkin the code and add comment for this check in.
Do you have problem with the android guide? can not continue to build?
Hi,
I has asked IMX6 FAE in china , this print info is good, not an error: I has got the correct branch kernel & uboot of imx6.
I could build all Android L5.0.1 ok: after compile, I could get boot-imx6q.img, recovery-imx6q.img, system.img , u-boot-imx6q.imx.
there is another problem when I burn thease img into emmc on I.MX 6 Series SABREE board.
Steps:
1. I push thease img into mfgtools\Profiles\Linux\OS Firmware\files\android\sabresd (mfgtools for Android L5.0.0.1 is download form Freescale website)
2. Set SW6 into burn model, so mfgtool will show "HID xxx" info
3. double click "mfgtool2-android-mx6q-sabresd-emmc.vbs"
4. uart will print thease info, but mfg tool will pause, will not continue to burn img files:
Starting kernel ...
Booting Linux on physical CPU 0x0
Linux version 3.10.53-1.1.0_ga-mfgtool+g496fbe0 (jenkins@scmbl1) (gcc version 4.8.2 (GCC) ) #1 SMP Mon Jan 5 14:49:15 CST 2015
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 Quad SABRE Smart Device Board
cma: CMA: reserved 320 MiB at 3c000000
Memory policy: ECC disabled, Data cache writealloc
PERCPU: Embedded 8 pages/cpu @81528000 s8768 r8192 d15808 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260096
Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= enable_wait_mode=off
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 1024MB = 1024MB total
Memory: 690500k/690500k available, 358076k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xc0800000 - 0xff000000 (1000 MB)
lowmem : 0x80000000 - 0xc0000000 (1024 MB)
modules : 0x7f000000 - 0x80000000 ( 16 MB)
.text : 0x80008000 - 0x80c0862c (12290 kB)
.init : 0x80c09000 - 0x80c5b240 ( 329 kB)
.data : 0x80c5c000 - 0x80cad180 ( 325 kB)
.bss : 0x80cad180 - 0x80d0f714 ( 394 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
Hierarchical RCU implementation.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
NR_IRQS:16 nr_irqs:16 16
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
CPU identified as i.MX6Q, silicon rev 1.5
Console: colour dummy device 80x30
Calibrating delay loop... 789.70 BogoMIPS (lpj=3948544)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x80639f00 - 0x80639f58
CPU1: Booted secondary processor
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
Brought up 2 CPUs
SMP: Total of 2 processors activated (1579.41 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
pinctrl core: initialized pinctrl subsystem
regulator-dummy: no parameters
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
Use WDOG2 as reset source
syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
vdd1p1: 800 <--> 1375 mV at 1125 mV
vdd3p0: 2800 <--> 3150 mV at 3000 mV
vdd2p5: 2000 <--> 2750 mV at 2425 mV
cpu: 725 <--> 1450 mV at 975 mV
vddpu: 725 <--> 1450 mV
vddsoc: 725 <--> 1450 mV at 1175 mV
syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered
syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
bio: create slab <bio-0> at 0
mxs-dma 110000.dma-apbh: initialized
usb_otg_vbus: 5000 mV
usb_h1_vbus: 5000 mV
wm8962-supply: no parameters
mipi_dsi_pwr_on: no parameters
sensor-supply: 3300 mV
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
i2c i2c-1: IMX I2C adapter registered
i2c i2c-2: IMX I2C adapter registered
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
cfg80211: Calling CRDA to update world regulatory domain
pureg-dummy: no parameters
Switching to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP: reno registered
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 7160K (82c01000 - 832ff000)
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
imx6_busfreq busfreq.16: DDR medium rate not supported.
Bus freq driver module loaded
futex hash table entries: 512 (order: 3, 32768 bytes)
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.22)
msgmni has been set to 2002
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: WEIM driver registered.
mxc_mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed
MIPI DSI driver module loaded
mxc_sdc_fb fb.31: registered mxc display driver ldb
imx-ipuv3 2800000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
Console: switching to colour frame buffer device 128x48
mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1
fbcvt: 1920x1080@60: CVT Name - 2.073M9
mxc_sdc_fb fb.32: registered mxc display driver hdmi
mxc_sdc_fb fb.33: registered mxc display driver lcd
mxc_sdc_fb fb.33: ipu0-di0 already in use
mxc_sdc_fb: probe of fb.33 failed with error -16
mxc_sdc_fb fb.34: registered mxc display driver ldb
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: loaded firmware 1.1
imx-sdma 20ec000.sdma: initialized
pfuze100-regulator 1-0008: unrecognized pfuze chip ID!
pfuze100-regulator: probe of 1-0008 failed with error -5
Serial: IMX driver
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
console [ttymxc0] enabled
serial: Freescale lpuart driver
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
Wait for CR ACK error!
sata phy RX_PLL is stable!
ahci: SSS flag set, parallel bus scan disabled
ahci ahci: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst
scsi0 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 71
m25p80 spi32766.0: found mr25h256, expected m25p32
m25p80 spi32766.0: mr25h256 (32 Kbytes)
spi_imx 2008000.ecspi: probed
fec 2188000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00
fec 2188000.ethernet (unregistered net_device): Using random MAC address: fa:da:77:af:1f:53
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
usbcore: registered new interface driver usb-storage
ci_hdrc ci_hdrc.1: doesn't support gadget
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
elan-touch 2-0010: elan - Read Hello Packet Failed
elan-touch: probe of 2-0010 failed with error -22
egalax_ts 1-0004: Failed to read firmware version
egalax_ts: probe of 1-0004 failed with error -5
egalax_ts 2-0004: Failed to read firmware version
egalax_ts: probe of 2-0004 failed with error -5
input: max11801_ts as /devices/soc0/soc.1/2100000.aips-bus/21a4000.i2c/i2c-1/1-0048/input/input0
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
i2c /dev entries driver
mxc_v4l2_output v4l2_out.39: V4L2 device registered as video16
mxc_v4l2_output v4l2_out.39: V4L2 device registered as video17
mxc_v4l2_output v4l2_out.39: V4L2 device registered as video18
ata1: SATA link down (SStatus 0 SControl 300)
mxc_v4l2_output v4l2_out.39: V4L2 device registered as video19
mxc_v4l2_output v4l2_out.39: V4L2 device registered as video20
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
mag3110 2-000e: check mag3110 chip ID
mag3110 2-000e: read chip ID 0xfffffffb is not equal to 0xc4!
mag3110: probe of 2-000e failed with error -22
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
mma8451 0-001c: read chip ID 0x1 is not equal to 0x1a or 0x2a!
mma8451: probe of 0-001c failed with error -22
imx2-wdt 20c0000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
cpuidle: using governor ladder
cpuidle: using governor menu
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc1: no vqmmc regulator found
mmc1: no vmmc regulator found
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
mmc2: no vqmmc regulator found
mmc2: no vmmc regulator found
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
mmc3: no vqmmc regulator found
mmc3: no vmmc regulator found
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
Galcore version 5.0.11.25762
this info will not grow in a hour....
5. But I use "Mfgtools-Rel-1.1.0_121218_MX6Q_UPDATER " to burn Android 4.4.2 into the same board. It work ok. After I swithc SW6 to boot model, Android 4.4.2 run good.
6. If I only change cfg.ini like this, then click "MfgTool2.exe" to burn Android L5.0.0.1, It is same with running "mfgtool2-android-mx6q-sabresd-emmc.vbs".
default cfg.ini is :
default cfg.ini is:
[profiles]
chip = Linux
[platform]
board = SabreSD
[LIST]
name = SDCard
[variable]
board = sabresd
mmc = 0
sxuboot=17x17arm2
sxdtb=17x17-arm2
ldo=
I only change cfg.ini to test, like this:
[profiles]
chip = Linux
[platform]
board = SabreSD
[LIST]
name = eMMC-Android-IMX6Q-SabreSD
[variable]
board = sabresd
mmc = 0
ldo=
more information:
The Test Board is Fresscale IMX6 Official Demo board, we got this board from Freescle (we do not changing anything)
Android 4.4.2 burn model & boot mode work good with EMMC Flash(4GB).
But Android L5.0.0.1 burn model do not work.
I do not know the detail reason, Could you help me ? Could you burn img downloaded from Freescale websit into emmc Freescale board?
my PC is windows xp , will it affect ?
Best regards,
Hi all
I has found the reason: usb otg host/device switch
The Test Board is Fresscale IMX6 Official Demo board we has add a hardware switch for otg host or device.
we use this hardware as usual: download Android 4.4.2 ok, but dowload Android 5.0.2 failed.
Today, I remove this hardware switch, yes, download Android 5.0.2 ok , After I set SW6 to boot model, power on board, Android 5.0.2 show good.
Best regards
Hello Cagatay Buyuktopcu,
I reproduced this behavior and it’s not so much an error but a notice. After the last command you’re checking out the branch so you can work locally. Any changes made won’t be updated on the git servers.
You should be able to follow up with patching the source code after this. Please let us know if you encounter errors when patching the code.
Sidenote: Just in case any community user what’s to follow these steps, these are also listed on the Android User’s Guide. After checkout android-4.4.3_r1 you would need to go back to home with cd ~ in order for cd myandroid to work.
Hi,
when I update uboot-imx branch "l5.0.0_1.0.0-ga", follow by Android User’s Guide Rev. L5.0.0_1.0.0-ga, 06/2015
[19:17:36]yfb04@goldingmedia-imx6:~/myandroid/bootable/bootloader$ git clone git://git.freescale.com/imx/uboot-imx.git uboot-imx
[19:17:36]Cloning into 'uboot-imx'...
[19:18:02]remote: Counting objects: 324783, done.
[19:18:07]remote: Compressing objects: 100% (72869/72869), done.
[19:26:14]remote: Total 324783 (delta 259994), reused 310611 (delta 246015)
[19:26:14]Receiving objects: 100% (324783/324783), 75.67 MiB | 387 KiB/s, done.
[19:26:20]Resolving deltas: 100% (259994/259994), done.
[19:26:39]yfb04@goldingmedia-imx6:~/myandroid/bootable/bootloader$ ls
[19:26:39]legacy uboot uboot-imx
[19:26:43]yfb04@goldingmedia-imx6:~/myandroid/bootable/bootloader$ cd uboot-imx/
[19:26:51]yfb04@goldingmedia-imx6:~/myandroid/bootable/bootloader/uboot-imx$ git checkout l5.0.0_1.0.0-ga
[19:26:52]Note: checking out 'l5.0.0_1.0.0-ga'.
[19:26:52]
[19:26:52]You are in 'detached HEAD' state. You can look around, make experimental
[19:26:52]changes and commit them, and you can discard any commits you make in this
[19:26:52]state without impacting any branches by performing another checkout.
[19:26:52]
[19:26:52]If you want to create a new branch to retain commits you create, you may
[19:26:52]do so (now or later) by using -b with the checkout command again. Example:
[19:26:52]
[19:26:52] git checkout -b new_branch_name
[19:26:52]
[19:26:52]HEAD is now at 9d7bf9b... MA-6580 recovery.img cannot be authenticated by HAB
when I update kernel-imx branch "l5.0.0_1.0.0-ga", follow by Android User’s Guide Rev. L5.0.0_1.0.0-ga, 06/2015
$ git clone git://git.freescale.com/imx/linux-2.6-imx.git kernel_imx # the kernel repo is
large. Therefore, this process can take a while.
$ cd kernel_imx
$ git checkout l5.0.0_1.0.0-ga
yfb04@goldingmedia-imx6:~/myandroid$ cd ~/myandroid/
yfb04@goldingmedia-imx6:~/myandroid$ cd kernel_imx/
yfb04@goldingmedia-imx6:~/myandroid/kernel_imx$ git checkout l5.0.0_1.0.0-ga
HEAD is now at 4f0dd92... Don't set console cflag to zero.
At last
I could get base version kernel_imx & uboot-imxt (git clone ok)
I can not get the l5.0.0_1.0.0-ga brach uboot-imx & kernel-imx(git checkout l5.0.0_1.0.0-ga):
HEAD is now at 4f0dd92... Don't set console cflag to zero.
HEAD is now at 9d7bf9b... MA-6580 recovery.img cannot be authenticated by HAB
Could you help me to check what happened, Is my network bad, or I have the right limits of authority ?
Best regards,