Video property is as follows:
Topology:
container: Quicktime
audio: MPEG-4 AAC
video: H.264
Properties:
Duration: 0:15:20.810000000
Seekable: yes
Tags:
video codec: H.264 / AVC
maximum bitrate: 3695752
bitrate: 749856
audio codec: MPEG-4 AAC audio
language code: en
datetime: "2013-07-05T14:54:42.000000+0530"
container format: ISO MP4/M4A
If we play video using palybin, subtitle not displaying completely. Subtitle is getting cropped.
We observed, aiurdemux giving height=502 and vpudec giving height=512 and crop bottom set to 10.
So subtitle in bottom is getting cropped.
Video is uploaded in FTP at path : /data/From_Allgo_To_FSL/video
We are using gst-fsl-plugins version 3.5.7 and gstreamer version 10.36
Result of "uname -a" is
Linux freescale 3.0.35-2154-g94689e1 #180 SMP PREEMPT Wed Mar 4 15:24:49
CST 2015 armv7l GNU/Linux
BSP version is 3.0.35 based customized BSP.
Board is IM6D based customized board .
This is very urgent, for a production program. SOP is very close.
Please help us analysing this ASAP.
Regards:
Ramakrishna Kamath
Original Attachment has been moved to: video_crop_log.txt.zip
Original Attachment has been moved to: gst_log.txt.zip
This is due to hardware limitation, the IPU require 8 pixels align, so the video was cropped several lines.
best regards
Jack