Hello,
Our goal is to develop a demonstration application for various SPI, I2C and UART peripherals.
We would like to use a TWR-K70F120 board with a twr-lcd module for the display
This doesn't sound to be an unusual combination since the K70 has a built-in display controller but:
As far as support for PE goes we are a bit lost.
PE supports a peripheral driver LCDC but it looks like there is no GUI library supporting this driver as a back end.
EGUI is a free library, has an example for the K70, but only for an IAR compiler - we are using Kinetis Design Studio.
The documentation for the TWR-LCD demo applications mentiones a processor expert component library to import - but I cannot find it anywhere.
There is a PEG software solution available but it is not clear to me whether or not it is necessary to actually purchase a license when using it with a Kinetis controller - the license description is somewhat contradicting. In addition it is not mentioned that this library will integrate with PE.
So the question is:
Is there any (preferably Processor expert based) support for the K70 display controller in terms of basic GUI elements?
TIA, Roland
Hello Roland,
Does this thread can help you ? TWR-K70 + TWR-LCD-RGB demo projects
Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------