I need to build on a server that would do automated builds, checking and run unit tests.
is there anyway to get Pex to play nicely?
Or do I have to check in my generated code?
environment;
KDS
K20
GCC
Hello Keith,
The PEx in eclipse (KDS) support the following Command Line Interface (it is also described in the Help, see Processor Expert Software > Kinetis Design Studio > Processor Expert User Guide > User Interface > Command Line Interface).
Processor Expert provides a simple command line interface which can be used to generate output of PEx projects in an Eclipse workspace.
The CLI is implemented using a headless (without GUI) Processor Expert application. The headless application ID is:
Headless PEx application ID: com.freescale.processorexpert.core.PExApplication
The headless application can be run with these parameters:
- Generate code of all Processor Expert projects in a workspace: -generateAll - Generate code of a particular Processor Expert project in a workspace: -generate <projec name>
Examples:
eclipsec.exe -noSplash -data c:\Users\XYZ\workspace -application com.freescale.processorexpert.core.PExApplication -generate projectABC
eclipsec.exe -noSplash -data c:\Users\XYZ\workspace -application com.freescale.processorexpert.core.PExApplication –generateAll
Best Regards,
Marek Neuzil
Hi Keith,
there is a command line mode you can use to generate the Processor Expert code:
Eclipse Command Line Code Generation with Processor Expert | MCU on Eclipse
I hope this helps,
Erich