AnsweredAssumed Answered

Methods to allocate EBA for IDMAC in IPU

Question asked by Pradeepa Senanayake on Jun 12, 2015
Latest reply on Jun 12, 2015 by igorpadykov

Hello,

 

In the Linux kernel source the EBA for IPU-CPMEM is allocated using the dma_alloc_coherent API. Is this a must to do?

 

I'm writing a driver from the scratch for a very specific CSI module manipulation and therefore I would like to know whether there are any other ways to perform this memory allocation (ie. kmalloc).

 

In SDK the memory used for the EBA is,

 

#define IPU_DMA_MEMORY_START0x40000000

 

#define CH0_EBA1(IPU_DMA_MEMORY_START + 0x01C00000)

 

Do these memory locations have any special attributes associated or can I use any memory location by allocating through kmalloc?

 

Can someone give me some thought for this?

 

Thank you in advance.

Pradeepa

Outcomes