AMIC doesnot work on SABRESD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AMIC doesnot work on SABRESD

425 Views
vijaikumar
Contributor III

Hi all,

         We are using 3.14.28 kernel with i.MX6Q sabresd board. When trying to record audio via AMIC, the file is generated, however we are unable to hear anything. We are following the procedure mentioned in Linux User manual provided by freescale. Am I missing something?

$GSTL alsasrc num-buffers=430 blocksize=4096 ! imxmp3enc ! filesink location=output.mp3

Labels (2)
Tags (4)
0 Kudos
1 Reply

339 Views
igorpadykov
NXP Employee
NXP Employee

HI Vijai

one can refer to attached Porting Guide

Chapter 8 Porting Audio Codecs to a Custom Board

Also one can check hardware with SDK audio example

i.MX 6Series Platform SDK  : Bare-metal SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos