AnsweredAssumed Answered

CAN_LDD component not working on trk-kea128

Question asked by Laura Sanz on Jun 12, 2015
Latest reply on Jan 28, 2016 by Alice_Yang

Hello,

 

We are making some tests with the CAN component for a current project on codewarrior 10.6 but we are unable to make it work. We are using the KEAZ128 and the code copied from processor expert's typical usage section.

 

can1.PNG

 

After we set up the CAN config we implement the code from "Sending data frame without interrupt service (polling)" and run the program. Everything goes OK until it reaches the CAN1_Main() function. When the CAN1_Main() function calls the CAN1_TransmitterIsr() function the TxBufferMask never changes from 0 value, so it never ends the transmission of the data.

 

can2.PNG

 

Maybe we are using the wrong code but we couldn't find any working example of the CAN_LDD component for the KEAZ128.

Outcomes