mpc8260A FCC做网口时,什么情况下会停止发送数据呢?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mpc8260A FCC做网口时,什么情况下会停止发送数据呢?

544 Views
dzz870529
Contributor I

1.       FCC在什么情况下会停止发送?

2.       FCC在停止发送的时候可能报告什么错误信息?

3.       FCC的收发是否会受到MCC的影响?

下面是日志:

-> dxfDebugShow

unit 0 bds status

     tx bd:

     NO.     addr   length   buffer   status

     _______________________________________

     15   8000078       36  8019d04     7c00 (PAD,Wrap,Int,Last,Tx CRC)

     rx bd:

     NO.     addr   length   buffer   status

     _______________________________________

     31   8000178        0  8012740     a000 (Empty,Wrap)

unit 1 bds status

     tx bd:

     NO.     addr   length   buffer   status

     _______________________________________

     00   80c9000       4a  80cb2a0     dc00 (Ready,PAD,Int,Last,Tx CRC)

     01   80c9008       4a  80cac6c     dc00 (Ready,PAD,Int,Last,Tx CRC)

     02   80c9010       4a  80ca638     dc00 (Ready,PAD,Int,Last,Tx CRC)

     03   80c9018       4a  80d6cb8     dc00 (Ready,PAD,Int,Last,Tx CRC)

     04   80c9020       3c  80d6684     dc00 (Ready,PAD,Int,Last,Tx CRC)

     05   80c9028       3c  80d6050     dc00 (Ready,PAD,Int,Last,Tx CRC)

     06   80c9030       4a  80d5a1c     dc00 (Ready,PAD,Int,Last,Tx CRC)

    07   80c9038       3c  80d8588     dc00 (Ready,PAD,Int,Last,Tx CRC)

     08   80c9040       3c  80d4780     dc00 (Ready,PAD,Int,Last,Tx CRC)

     09   80c9048       3c  80d3b18     dc00 (Ready,PAD,Int,Last,Tx CRC)

     10   80c9050       3c  80d34e4     dc00 (Ready,PAD,Int,Last,Tx CRC)

     11   80c9058       3c  80d2eb0     dc00 (Ready,PAD,Int,Last,Tx CRC)

     12   80c9060       4a  80cea74     dc00 (Ready,PAD,Int,Last,Tx CRC)

     13   80c9068       4a  80cf0a8     dc00 (Ready,PAD,Int,Last,Tx CRC)

     14   80c9070       4a  80cc53c     dc00 (Ready,PAD,Int,Last,Tx CRC)

     15   80c9078       4a  80d72ec     fc00 (Ready,PAD,Wrap,Int,Last,Tx CRC)

     rx bd:

     NO.     addr   length   buffer   status

     _______________________________________

     31   80c9178        0  80e07e0     a000 (Empty,Wrap)

value = 0 = 0x0

-> motFccDrvShow 1

unit 1 drv ctrl show

                      pDrvCtrl = 0x77b5168

                      pNetPool = 0x77b50b0

                     pClPoolId = 0x77f89f0

                       pBdBase = 0x80c9000

                        bdSize = 0x1000

                      pBufBase = 0x80ca000

                       bufSize = 0xc8000

                     pMBlkArea = 0x77b2e78

                      mBlkSize = 0x222c

                 fccIntPending = 0

                  fccRxPending = 0

                  fccTxPending = 0

                       tbdBase = 0x80c9000

                        tbdNum = 16

                      tbdIndex = 12

                  usedTbdIndex = 12

                   cleanTbdNum = 0

                       txStall = 0

                       rbdBase = 0x80c9080

                        rbdNum = 32

                      rbdIndex = 11

                   fccIramAddr = 0x47011340

                   fccPramAddr = 0x47008600

                        fccNum = 3

fcc tx and rx error show

                        nTxErr = 0x0

                         RxBsy = 0x4

                         nTxLc = 0x0

                          TxUr = 0x0

                         TxCsl = 0x0

                          TxRl = 0x0

                         nRxLg = 0x0

                          RxNo = 0x0

                         RxCrc = 0x0

                          RxOv = 0x0

                          RxLc = 0x0

                          RxSh = 0x0

                        nRxMem = 0x6eb96

-> motFccRamShow 1

unit 1 Iram show

                          gfmr = 0x2000003c

                         fpsmr = 0x14000080

                         ftodr = 0x1400

                          fdsr = 0xd555

                         fccer = 0x0

                         fccmr = 0xfe

unit 1 Pram show

                         RIPTR = 0xb0a0

                         TIPTR = 0xb040

                         MRBLR = 0x5ee

                        RSTATE = 0x13810000

                         RBASE = 0x80c9080

                        RBDLEN = 0x0

                         RDPTR = 0x80d7f60

                        TSTATE = 0x1340001d

                         TBASE = 0x80c9000

                        TBDLEN = 0x4a

                         TDPTR = 0x80db728

                         RBPTR = 0x80c90c0

                         TBPTR = 0x80c9068

                   retry limit = 0xf

-> motFccRamShow 1

unit 1 Iram show

                          gfmr = 0x2000003c

                         fpsmr = 0x14000080

                         ftodr = 0x1400

                          fdsr = 0xd555

                         fccer = 0x0

                         fccmr = 0xfe

unit 1 Pram show

                         RIPTR = 0xb0a0

                         TIPTR = 0xb040

                         MRBLR = 0x5ee

                        RSTATE = 0x13a00000

                         RBASE = 0x80c9080

                        RBDLEN = 0x5a

                         RDPTR = 0x80e45e0

                        TSTATE = 0x1340001d

                         TBASE = 0x80c9000

                        TBDLEN = 0x4a

                         TDPTR = 0x80db728

                         RBPTR = 0x80c90f8

                         TBPTR = 0x80c9068

                   retry limit = 0xf

-> motFccRamShow 1

unit 1 Iram show

                          gfmr = 0x2000003c

                         fpsmr = 0x14000080

                         ftodr = 0x1400

                          fdsr = 0xd555

                         fccer = 0x0

                         fccmr = 0xfe

unit 1 Pram show

                         RIPTR = 0xb0a0

                         TIPTR = 0xb040

                         MRBLR = 0x5ee

                        RSTATE = 0x13a00000

                         RBASE = 0x80c9080

                        RBDLEN = 0x9a

                         RDPTR = 0x80e7dc0

                        TSTATE = 0x1340001d

                         TBASE = 0x80c9000

                        TBDLEN = 0x4a

                         TDPTR = 0x80db728

                         RBPTR = 0x80c90c8

                         TBPTR = 0x80c9068

                   retry limit = 0xf

_________________________________

邸学锋

0 Kudos
1 Reply

472 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello ding ding,

Please analyze whether there could be external cause of this issue(PHY), you could reset the FCC by issuing STOP_TX, init the FCC Dpram, issuing INIT_TX_PARAMS, and RESTART_TX.

You could refer to FCCE, which should indicates a reason for FCC stopping. And also inspect TxBDs status bits.

Each FCC FIFO has threshold values, determined by the mode it is using, for determining normal and emergency CPM request prioritization. When an FCC is in emergency mode, that FCC's TX or RX request may have higher priority than MCC TX or RX. When FCC1 in particular is in emergency priority mode, it will always be of higher priority than an MCC. This opens up the possibility of the FCC starving out the MCC if the FCC continues to be over utilized. This can lead to a GUN. To help alleviate this situation, setting FPSMR[TPRI] prevents the FCC’s TX from going into emergency mode and can minimize the risk of global underrun


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos