AnsweredAssumed Answered

can't flash K64F because no msd under linux

Question asked by Dave Boyle on Jun 9, 2015
Latest reply on Jun 11, 2015 by Hui_Ma

I'm using KDS 3.0 to debug a FRDM-K64F under Ubuntu 14.04 and when I plug in the usb cable I do NOT see a mass storage device. I'm supposed to see one named K64F. This has not been a problem because I have been debugging out of KDS 3.0 with the Segger connection and it works fine. Getting closer to deployment though, I need to run the board stand-alone but the code won't work unless it's running in a debug session.

 

Flashing it from inside KDS doesn't work so I went to drop the .bin file onto the msd but it's not there. I tried the P&E Micro connection but it won't show an msd either. I feel trapped in a box! In desperation I wrote this description of the problem on the web forum so hopefully someone can help me!

Outcomes