AnsweredAssumed Answered

4 Channel 720P30 Video capture with single Soc

Question asked by Shabbir Limdiwala on Jun 5, 2015
Latest reply on Aug 13, 2015 by Qiang Li - Mpu Se

Hi,

 

For one of the upcoming products, we are looking for right architecture to implement SVM (Surround view monitoring) system. There will be 4 cameras mounted on car's front, rear, left and right side and we want to design a host system which can capture 4 channel Bayer/YUV data (each 720P@30), stitch them together to create one 720P view to be displayed on dashboard.

 

Can you suggest Freescale SoC which is able to capture 4 simultaneous channel 720P@30 fps?

If I am not wrong, one i.mx6 can capture two 720P30 channels at max. What if I want to capture 4 channels (I am fine using either CSI/paralle/both interfaces to achieve this use case).

 

If single SoC can't do that, what are the possible ways to achieve this use case?

 

Regards,
Shabbir

Outcomes