AnsweredAssumed Answered

imx6qsabreauto ping test

Question asked by LEE SEUNGHYUN on Jun 4, 2015
Latest reply on Jun 8, 2015 by LEE SEUNGHYUN

Hi,  I am working on sabre auto board and wanted to test the Ping.

but..it was not well.

 

- First, download the BSP source. In order to using yocto project. see  https://community.freescale.com/docs/DOC-94849

 

- and , build:  $ bitbake fsl-image-gui .

- Deploy the sdcard image:  $ sudo dd if=fsl-image-gui-imx6qsabresd.sdcard of=/dev/sdX bs=1M

 

- My sd Card in the correct board's and boot

-----------------------------------------------------------------------------

- my computer ip setting

ifconfig eth0 192.168.10.100 netmask 255.255.255.0

route add default gw 192.168.10.1

 

- imx6 ip setting

ifconfig eth0 192.168.10.102 netmask 255.255.255.0

route add default gw 192.168.10.1

-----------------------------------------------------------------------------

test the ping is not well.

Do you ever need a different setting?

help me.

.

Outcomes