MMPF0100 VGEN4 1.8V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMPF0100 VGEN4 1.8V

Jump to solution
684 Views
sylvia
Contributor I

Hi Community

We had received Default Configuration of MMPF0100, The default voltage at VGEN4 is not got. All other regulator outputs are proper.

Kindly suggest what may be the issue. The  input to PMIC (VIN) is 3.4V. If suppose we power up the PMIC through Battery , the input Voltage will go upto 4.2 V.

Is there any proplem for the regulators, since VGEN4 Input regulator VIN max is 3.6 V???

Thanks and Regards

Sylvia

Tags (1)
0 Kudos
1 Solution
546 Views
Yuri
NXP Employee
NXP Employee

  Please check Your design regarding the Startup erratum

(False start and/or non-start of regulators).

http://cache.freescale.com/files/analog/doc/errata/MMPF0100ZER.pdf


Have a great day,
Yuri
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
547 Views
Yuri
NXP Employee
NXP Employee

  Please check Your design regarding the Startup erratum

(False start and/or non-start of regulators).

http://cache.freescale.com/files/analog/doc/errata/MMPF0100ZER.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos