I found this in imx6qdl.dtsi
uart2: serial@021e8000 {
compatible = "fsl,imx6q-uart", "fsl,imx21-uart";
reg = <0x021e8000 0x4000>;
interrupts = <0 27 0x04>;
clocks = <&clks 160>, <&clks 161>;
clock-names = "ipg", "per";
dmas = <&sdma 27 4 0>, <&sdma 28 4 0>;
dma-names = "rx", "tx";
status = "disabled";
};
To use UART2, editing status "enabled" is needed, I think.
What is next step? 'i.MX_6_Linux_Reference_Manual.pdf' just says imx.c is driver file and it has no example for init port, tx data, rx interrupt.
Maybe sabre board can access GPS module via UART, please tell me at least where is the source file for GPS DATA collecting.
ps)3.0.xx BSP has this routine. Does 3.10.53 have similar one?
---------------------------------------------------------------
static inline void mx6q_sabresd_init_uart(void)
{
imx6q_add_imx_uart(2, NULL);
imx6q_add_imx_uart(0, NULL);
}
---------------------------------------------------------------
Solved! Go to Solution.
Hi JHY
for uart configs one can look at attached Linux Manual
sect.47.3.4 Board Configuration Options,
also please check uart2 pinctrl settings, like in example below
[meta-freescale] [meta-fsl-arm-extra][PATCH v2 4/4] linux-compulab: ad
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi JHY
for uart configs one can look at attached Linux Manual
sect.47.3.4 Board Configuration Options,
also please check uart2 pinctrl settings, like in example below
[meta-freescale] [meta-fsl-arm-extra][PATCH v2 4/4] linux-compulab: ad
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------