AnsweredAssumed Answered

flash: no space left on device

Question asked by Niklas Molin on Jun 1, 2015
Latest reply on Jun 2, 2015 by CarlosCasillas

Hi.

 

I'm running an image on an i.mx6D (build int Yocto).

The image is running from an emmc (Flash) which is around ~16Gb.

When I try to copy some files to the flash (via SSH) I get following problem:

 

/home/root/nodeJs/.......: No space left on device

 

 

I check the size of the disk with df -h, it there should be space left

 

Filesystem      Size  Used Avail Use% Mounted on

/dev/root        15G  9.5G  4.1G  70% /

devtmpfs        342M  4.0K  342M   1% /dev

tmpfs           502M  164K  502M   1% /run

tmpfs           502M   43M  460M   9% /var/volatile

/dev/mmcblk0p1  8.0M  8.0M   24K 100% /media/mmcblk0p1

 

Is there some setup I need to do to tell it that we are using 16 Gb disk when I compile or maybe some config file under /etc?

 

Thanks,

Niklas

Outcomes