Hello,
Can I access serial port on TWR-Ser2 from Timesys? It is ttyc: on MQX but I need to access if from Timesys
This is from straight C. I have the code but need to know the name of the port on the TimeSys side.
thanks
Thomas
Solved! Go to Solution.
Hello Thomas,
The serial console in Linux enumerates as ttymxc1; in the 3.13 kernel the driver is located at /drivers/tty/serial/imx.c
Regards,
Timesys Support
Hello Thomas,
The serial console in Linux enumerates as ttymxc1; in the 3.13 kernel the driver is located at /drivers/tty/serial/imx.c
Regards,
Timesys Support
great! thanks
timesyssupport can you attend this case?
Timesys Support do you have an update?