I am running the hello2 example project and the idle task is not running, so when the 2 tasks in the example both block, the CPU goes to an dead loop with the comment
/* woohoo, idle task must be enabled, this point cannot be reachable, you have serious problem */
I have MQX_USE_IDLE_TASK set to 1 in my user_config.h
I can follow the pointer kernel_data->IDLE_LOOP and see the code for _mqx_idle_task() is in memory, but that code never runs.
Any ideas?
I have the same problem.
My hardware is a custom board with kinetis k30 (MK30DX256VLK7).
Can anyone help me?
With Best Regards
Hi James
has your problem been resolved?
Best Regards,
Isaac
Hi James,
Which hardware platform (Tower or Freedom or custom (but what device used)) and IDE used?
Regards,
David