AnsweredAssumed Answered

Can single i.MX6 LVDS support 1920x1080 30 Hz?

Question asked by Antti Toivonen on May 29, 2015
Latest reply on May 31, 2015 by igorpadykov

Is it possible to simultaneously drive three independent displays at the same time with i.MX6:

- HDMI 1920x1080 60 Hz

- LVDS0 1920x1080 30 Hz

- LVDS1 1920x1080 30 Hz

 

Documentation does not give a clear answer, just mentions 1366x768 @ 60 Hz / 85 MHz maximum for single-channel LVDS. 1920x1080 @ 30 Hz should have pixel clock of 74 MHz which is within the specification but are there other limitations?

Outcomes