Completion flag rarely NOT assert when i.MX53 FEC MII recieve completed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Completion flag rarely NOT assert when i.MX53 FEC MII recieve completed

Jump to solution
477 Views
torus1000
Contributor V

Dear Expert-team,

FEC_EIR[23](MII interrupt) rarely NOT assert when i.MX53 FEC MII data recieve (or read reg of PHY) completed.
If this happend, communication force disconnected.  It was clearly not satisfied our product requirements.

Why didn't FEC_EIR[23] flag changed?

Is there any workaround for this?

Thanks.

Labels (1)
0 Kudos
1 Solution
392 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

one can try to check if this is caused by FEC FIFO overrun issue,

that is FEC DMA cannot access ddr in time:

1, Prioritize the master via M4IF.

      Increase FEC priority:

            0x63fd_8044=0x33

            0x63fd_8048=0x1901a3

2, Increase FEC RX FIFO size.

      RX FIFO size = 1.5*(orginal size) => 0x63fe_c150=0x480

      RX FIFO size = 1.625*(orginal size) => 0x63fe_c150=0x460

      The result as below table, and the patch as below.

Kernel Patch:

--- a/drivers/net/fec.c

+++ b/drivers/net/fec.c

@@ -1300,6 +1300,11 @@ fec_restart(struct net_device *dev, int duplex)

               writel(0, fep->hwp + FEC_HASH_TABLE_LOW);

#endif

+             /* Set RX FIFO */

+#ifdef CONFIG_ARCH_MX53

+             writel(0x480, fep->hwp + FEC_R_FSTART);

+#endif

+

               /* Set maximum receive buffer size. */

               writel(PKT_MAXBLR_SIZE, fep->hwp + FEC_R_BUFF_SIZE);

Uboot patch:

--- a/board/freescale/mx53_smd/lowlevel_init.S

+++ b/board/freescale/mx53_smd/lowlevel_init.S

@@ -81,6 +81,17 @@

           beq 1b

.endm

+/* M4IF setup */

+.macro init_m4if

+          ldr r0, =M4IF_BASE_ADDR

+

+          ldr r1, =0x33

+          str r1, [r0, #0x44]

+

+          ldr r1, =0x001901A3

+          str r1, [r0, #0x48]

+.endm /* init_m4if */

+

.macro init_clock

           ldr r0, =ROM_SI_REV

           ldr r1, [r0]

@@ -218,6 +229,8 @@ lowlevel_init:

           init_l2cc

           init_aips

+        

+          init_m4if

            init_clock

Best regards

igor
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
393 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

one can try to check if this is caused by FEC FIFO overrun issue,

that is FEC DMA cannot access ddr in time:

1, Prioritize the master via M4IF.

      Increase FEC priority:

            0x63fd_8044=0x33

            0x63fd_8048=0x1901a3

2, Increase FEC RX FIFO size.

      RX FIFO size = 1.5*(orginal size) => 0x63fe_c150=0x480

      RX FIFO size = 1.625*(orginal size) => 0x63fe_c150=0x460

      The result as below table, and the patch as below.

Kernel Patch:

--- a/drivers/net/fec.c

+++ b/drivers/net/fec.c

@@ -1300,6 +1300,11 @@ fec_restart(struct net_device *dev, int duplex)

               writel(0, fep->hwp + FEC_HASH_TABLE_LOW);

#endif

+             /* Set RX FIFO */

+#ifdef CONFIG_ARCH_MX53

+             writel(0x480, fep->hwp + FEC_R_FSTART);

+#endif

+

               /* Set maximum receive buffer size. */

               writel(PKT_MAXBLR_SIZE, fep->hwp + FEC_R_BUFF_SIZE);

Uboot patch:

--- a/board/freescale/mx53_smd/lowlevel_init.S

+++ b/board/freescale/mx53_smd/lowlevel_init.S

@@ -81,6 +81,17 @@

           beq 1b

.endm

+/* M4IF setup */

+.macro init_m4if

+          ldr r0, =M4IF_BASE_ADDR

+

+          ldr r1, =0x33

+          str r1, [r0, #0x44]

+

+          ldr r1, =0x001901A3

+          str r1, [r0, #0x48]

+.endm /* init_m4if */

+

.macro init_clock

           ldr r0, =ROM_SI_REV

           ldr r1, [r0]

@@ -218,6 +229,8 @@ lowlevel_init:

           init_l2cc

           init_aips

+        

+          init_m4if

            init_clock

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos