AnsweredAssumed Answered

Enabling MRAM in MQX4.1 code.

Question asked by Praveen S on May 27, 2015

I am using mcf52259 controller and MQX4.1 RTOS.

I have MRAM on my Board and as said in main.h  i uncommented the below line

**************************************************************************************************************************************

/* Uncomment following code to use whole external MRAM for ramdisk, if available.

Not applicable when using MRAM target! */

 

 

#define RAM_DISK_BASE BSP_EXTERNAL_MRAM_BASE

#define RAM_DISK_SIZE BSP_EXTERNAL_MRAM_SIZE

********************************************************************************************************************************************

********************************************************************************************************************************************

Tried to use whole MRAM for ramdisk....

Then i flashed my code...

 

But in the console it is showing

 

Initialized RAMdisk to a:/

 

and getting stuck in the code ...

And Not moving further....

 

Can anyone suggest me a solution on this......

Original Attachment has been moved to: Testing_4.1.rar

Outcomes