AnsweredAssumed Answered

TWR-K60D100M

Question asked by Imran Khan on May 27, 2015
Latest reply on May 28, 2015 by Imran Khan

Hello Forum,

I just started using twr-k60d100m board for development, using USB cable to power on the board.

I have following setup:

1/ On Ubuntu 14.04 and Ubuntu 15.05 OS on the my desktop and notebook

2/ USB cable connected to the usb port and  system recognised usb port after lsusb command

  Bus 005 Device 003: ID 15a2:0058 Freescale Semiconductor, Inc.

3/ I am trying to upload/flash the program in to the board

4/ I have st-link and openocd utilities

5/ also downloaded P&E micro virtual usb driver.

6/ Do I still need the P&E USB Multilink Universal KIT to flash or upload an image/program?

7/ Just USB cable will not do? As I  tried several attempt but no result nor any sign that the image loaded?

 

I will be grateful if someone put me in right direction, please.

Thank you,

IK

Outcomes