I use the software of CW10.5. Now I want to add S29AL008J55BFIR2 in the MCF5253. I do it follow the document of AN3859. When I create a new target task, I add device to target task, I just find the S29AL008DB in the poped list. Need your help to check wether it's right for S29AL008J55BFIR2. If it's not the right one, can you show me which one I should select.
Hi,
This seems to be similar to the SR# 1-3832057904.
Below the answer sent ...
++++++++++++++++++++++++
The Flash_Programmer devices supported are listed under:
\MCU\bin\plugins\support\Flash_Programmer\ColdFire
\MCU\bin\plugins\support\Products\ProductData\ColdFireFPDevices.mwpdb\FP
If your device is not listed you must create it using the AN
http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN3859.pdf
I don't think you can use this flash config.
The S29AL008D and S29AL008J are not the same device type.
Please have a look at link:
http://www.spansion.com/Products/memory/parallel-flash/Pages/Spansion%20AL.aspx
Another important doc is at link:
http://www.spansion.com/Support/Related%20Product%20Info/S29AL008D_overview.pdf
Have a look page 2 to understand the device name definition for S29AL008D.
In Add Device list there are:
S29AL008DB
S29AL008DT
Difference is given by B and T which is defined by PACKAGE TYPE (T = TSOP Package B = Fine-pitch BGA Package).
++++++++++++++++++++++++
Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------