Hi,
i try to link my project with long long variables. Compile work fine but i can't link my project.
I get link errors like undifened : "__rt_divu64", undifined "__rt_or64" etc.
I tryed some librarys like C_TRK_4i_CF_FPU_StdABI_MSL.a but i get also the same errors from linker.
Can someone tell me which lib i need?
I use CodeWarrior 5.7.0
Thx.
Best Regards,
Georg.
Hi Georg,
Please try adding the standard library called “C_4i_CF_MSL.a”
I would also recommend you to use the latest Classic IDE v7.2:
CodeWarrior Development Tools for ColdFire|Freescale
Or the newest version of the eclipse based CodeWarrior 10.6:
CodeWarrior for Microcontrollers-Eclipse IDE|Freescale
On these versions of CodeWarrior those operations are enabled by default.
Hope it helps!
Best Regards,
Carlos Mendoza
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------