Open GL drivers for i.MX31 and i.MX53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Open GL drivers for i.MX31 and i.MX53

660 Views
paulschoenke
Contributor III

Hello:

I have some products that are in production with the Freescale i.MX31 and i.MX53 processors.  When we released these products, there were no Open GL drivers.

Are there Open GL drivers available now for either or both of these processors and if so, where can I get them?

Thanks!

Paul

Labels (1)
0 Kudos
1 Reply

503 Views
igorpadykov
NXP Employee
NXP Employee

Hi Paul

drivers can be found in BSPs on links below (please look at description in attached docs)

L2.6.35_11_09_ER_SOURCE : Linux 2.6.35 Source Code Files and documentation

11.09. Supports MCIMX53-START and MCIMX53-START-R.

IMX31_PDK15_LINUX_BSP  : Linux 2.6.26 Source Code Files for Release 1.5.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos