Hi,
We are using imx6Q SabreSD platform for our development with Linux3.14.28_1.0.0-GA BSP.
But initially we used Linux 3.10.17_1.0.0-GA BSP.
The Linux3.14.28_1.0.0-GA BSP uses "U-Boot-2014.04" and the Linux 3.10.17_1.0.0-GA BSP uses "U-Boot-2013.04" versions.
We have gone through below file in U-Boot-2014.04 and found that the "CONFIG_SYS_GENERIC_BOARD" macro is defined.
~/u-boot-imx/include/configs/mx6sabre_common.h
Because of the macro "CONFIG_SYS_GENERIC_BOARD" definition, the "board_init_f" and "board_init_r" functions are executed from the below files respectively.
~/u-boot-imx/common/board_f.c
~/u-boot-imx/common/board_r.c
But we have gone through below file in U-Boot-2013.04 and found that the "CONFIG_SYS_GENERIC_BOARD" macro is not defined.
~/u-boot-imx/include/configs/mx6qsabre_common.h
With U-Boot-2013.04, the "board_init_f" and "board_init_r" functions are executed from the below file
~/u-boot-imx/arch/arm/lib/board.c
From U-Boot-2014.04, why the "board_init_f" and "board_init_r" functions are not executed from below file.
~/u-boot-imx/arch/arm/lib/board.c
Please suggest us.
Thanks and Regards,
Ansari
Hi Abdul
this was discussed on uboot mailing list, you can post there if necessary
[U-Boot] about CONFIG_SYS_GENERIC_BOARD
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------