Where can i download the L5.0.0 Android Lollipop for imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can i download the L5.0.0 Android Lollipop for imx6

Jump to solution
1,027 Views
wilsonchen
Contributor III

Hi All,

       I found the imx6 L5.0.0 kernel and uboot code on the freescale'git server ,and I can download them.

But I can't find the Freescale Android L5.0.0 BSP on the public Freescale web site. I want to know when this will be release on the Freescale web site.

Thank you

Labels (4)
Tags (1)
0 Kudos
1 Solution
472 Views
igorpadykov
NXP Employee
NXP Employee

Hi wilson

android L5 GA release is planned on Jun 2015.

Best regards

igor
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
473 Views
igorpadykov
NXP Employee
NXP Employee

Hi wilson

android L5 GA release is planned on Jun 2015.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos