MQX + KDS + PE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX + KDS + PE

435 Views
profprogrammer
Contributor III

Hellow.

I am used  Processor Expert in BSP.

When I complying this project.  i get error.

..\Generated_Code\Cpu.c:206:7: error: expected '(' before 'void'

__asm void Cpu_SetBASEPRI(uint32_t Level) {

       ^

11:50:04 Build Finished (took 26s.557ms)

Why there is a mistake?

how to get rid of it?

Tags (1)
0 Kudos
1 Reply

230 Views
soledad
NXP Employee
NXP Employee

Hello,

Could you please specify which MQX version are you using?

Please check the attached document, and try to follow the steps in the page 42.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos