After pulling my hair out about why a current controller eTPU function wouldn't run, and after verifying it would properly execute a step if I used a host service request to invoke it, I just decided to change the channel it was running on to the same eTPU. It worked properly. I found that links from eTPU A to eTPU B don't work.
To make a long story short, I think where the application notes (this is from Analog Sensing for DC converters) say something like:
• CC_innerloop_chan (uint8_t) – Number of the channel on which an inner-loop controller (in slave mode) runs. In order to not activate any inner-loop controller, set the number to a channel with priority disabled. This parameter should be assigned a value of 0-31 for ETPU_A and of 64-95 for ETPU_B.
is not correct, I think this gets directly loaded into the link register:
+-------------------------------------------------------+
| Engine Select | Channel number |
+-------------------------------------------------------+
| 6 | 5 | 4 | 3 | 2 | 1 | 0 |
+-------------------------------------------------------+
0 0: Select this engine
0 1: Select engine A
1 0: Select engine B
1 1: Select other engine
and so 0-31 is Select this engine while 64-95 is Select engine B.
Am I right? Is this well-known? I had to dig into the eTPU reference manual to figure this out, which a consumer of the API in the application notes shouldn't need to do. Google searches didn't help.
Sorry, I meant links from eTPU B to eTPU don't work. Links to eTPU B work if you follow the API since it specifies Run on engine B. Link to eTPU A from eTPU B don't work because it specifies to run on the same engine.
So links A->A, A->B, B->B all would work, only B->A wouldn't work (using the channel number from the documentation).