Not starting after compiling android_kk4.4.3_2.0.0 on IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not starting after compiling android_kk4.4.3_2.0.0 on IMX6

Jump to solution
1,236 Views
andreylipov
Contributor II

Hello Dear Friends and all how can help me.

Sorry for my english.

Currently there is a problem, after compiling android 4.4.3_2.0.0 it does not run in more detail below.

A little background.

I have a board with IMX6Q from the company Embedsky.

Already in half a year I am trying to connect to her lcd, with another different frequency resolution, DE, clocks and other things.

Tries LVDS and parallel RGB, after a change always displays the old lcd settings (Default). My settings do not apply.

mxc_lcdif.c

board-mx6q_sabresd.c

ldb.c

And tried to change default LCD mxcfb_claa_wvga.c

nothing works, all to no avail

As I understand it, they hardcoded somewhere in the code standard monitor to their monitors purchased complete with the motherboard.

I decided to take the standard sources of freescale android 4.4.3_2.0.0

Downloaded android_kk4.4.3_2.0.0-ga_doc.tar.gz , then I configure the environment, and downloaded the source Android_User's_Guide.pdf

Successfully compiled assemblies for SabreSD, uploaded it to my motherboard.

but after connecting, nothing happens, not even comes to: Starting Kernel 

No erorrs....

If necessary I can provide logs, assembly, all necessary information.

I would be grateful for any help and tips.

Thank's a lot,

Andrey.

0 Kudos
1 Solution
700 Views
haoranwang
NXP Employee
NXP Employee

Hi,

     Which platform did you use?

     And did you flash the images into the storage like SD card or eMMC?

     Is the configuration-pin correct?

     Thanks.

BRs,

Haoran

View solution in original post

0 Kudos
2 Replies
701 Views
haoranwang
NXP Employee
NXP Employee

Hi,

     Which platform did you use?

     And did you flash the images into the storage like SD card or eMMC?

     Is the configuration-pin correct?

     Thanks.

BRs,

Haoran

0 Kudos
700 Views
andreylipov
Contributor II

Any Idies? :smileycry:

0 Kudos