Dear all,
we are using IMX6 Dual processor to run a Full HD Animated image in our TFT.
Now the image Frame rate 30 FPS.
Does our processor have the capability to run the same in 60 FPS?
NOTE:
1. In the Datasheet it has mentioned without "Multimedia Framework" the The video can be recorded and the same can be playbacked at 60 FPS.
Kinldy HELP:)
Regards,
Muthuraj M
+919003281838
Solved! Go to Solution.
Hi Muthuraj
typical value is 30fps as shown on presentation p.21
A Deep Dive into Image Processing for i.MX 6 Series Applications Processors
p.118 shows 60fps use case.
Performance depends om use case, since some IPU submodules are limited to 1920x1080 @ 30 fps,
sect.38.1.2.1.5.3 Image Converter (IC) IMX6SDLRM
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks a lot Igor:)
Hi Muthuraj
typical value is 30fps as shown on presentation p.21
A Deep Dive into Image Processing for i.MX 6 Series Applications Processors
p.118 shows 60fps use case.
Performance depends om use case, since some IPU submodules are limited to 1920x1080 @ 30 fps,
sect.38.1.2.1.5.3 Image Converter (IC) IMX6SDLRM
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
If the resolution about 640x480 60fps and data format is RGB888 from mipi-csi2, is it possible to preview in 60fps?