I use Atheros AR9K in i.mx6sl evk with ltib which use linux 3.0.35.
I set CONFIG_PCI, CONFIG_IMX_PCIE enabled.
The lspci command can work but no pci device displayed.
Any patch file about pcie existed for i.mx6 solo evk?
Solved! Go to Solution.
Hi yan
yes, it is used for some mini PCIe form-factor cards like:
UHMC-GNB-AR-01 (ARS63-SB / ARS63-S)
802.11gn+BT Coexistence Wireless Module
i.MX6SoloLite has not PCIe module.
~igor
Hi yan
i.MX6SoloLite has not PCIe module.
EVK has MINI PCI EXPRESS slot, it is used for some
WiFi cards which actually do not use PCIe.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor
Thank you for your reply.
I couldn't understand the means of "EVK has MINI PCI EXPRESS slot, it is used for some WiFi cards which actually do not use PCIe.".
I think EVK has mini PCIe slot, so it should be identified if a mini wifi pcie module be attached.
Hi yan
MINI PCI EXPRESS slot has also usb signals. They are used for some
WiFi cards made in mini PCIe connector form-factor.
Best regards
igor
Hi igor
Thank you for your reply. Do you mean the mini pcie slot in i.mx6sl evk only support usb signal and DO NOT support x1 PCI-E?
Both Mini PCI Express Form Factor and Express Card Form Factor support x1 PCI Express signals and USB and SMBus interfaces.
Any other form factor with the mini pcie slot in i.mx6sl evk?
Best Regards,
Yan
Hi yan
yes, it is used for some mini PCIe form-factor cards like:
UHMC-GNB-AR-01 (ARS63-SB / ARS63-S)
802.11gn+BT Coexistence Wireless Module
i.MX6SoloLite has not PCIe module.
~igor
Hi igor
Thank you for your information. I got it.
Best Regards,
Yan