AnsweredAssumed Answered

PMIC_STBY_REQ on MX6DL

Question asked by tony.l.cai on May 21, 2015
Latest reply on May 25, 2015 by igorpadykov

Dear All,

     Now I measured the Pin PMIC_STBY_REQ, I found when I plugged in the adapter, the pin output logical "1",when I power up, the Pin output the logical "0".and whatever the system in sleep state or in normal state, the pin output the logcal "0". And the spec said when the system entered into sleep state,the pin signal will transation from "1" to "0", the system exited the sleep state, the pin signal will transation from "1" to "0", so actually, I want to know how to control the pin?

Outcomes