AnsweredAssumed Answered

KSDK eMMC support

Question asked by Kevin Alden on May 21, 2015
Latest reply on Jun 9, 2016 by Wesley Hunter

Hello,

I am integrating a K65 with an eMMC chip.  I am using the K65 SDHC peripheral for this.  We had assumed that since the KSDK supports this peripheral that eMMC access would also be supported, but that does not seem to be the case.  The code detects the presence of an eMMC card and then returns a NOT_SUPPORTED_YET failure.  I investigated MQX 4.2, and while the code is different the behavior looks to be the same.

 

We are looking at modifying fsl_sdhc_card.c to support eMMC (or simply creating a emmc_card.c), but I was wondering if freescale has any plans to add this support to the SDK?

 

Thanks

Outcomes