Hi community,
I want to confirm what color format is usable for graphic combining in IPU.
According to IMX6DQRM (Rev.2), supported input format is written as below.
In chapter 37.1.2.1.4.2 (DP), "Format: YUVA/RGBA, non-decimated, 8 bits/value"
In chapter 37.1.2.1.5.2 (VDIC), "Pixel format: RGB/YUV 4:2:2, 8 bits/value"
In cahpter 37.1.2.1.5.3 (IC), "Pixel format: YUV/RGB, 8 bits/value"
[Q1]
I understand DP and IC can combine YUV444, YUV420, and YUV400 also since these format are less than 8 bits/value, right?
[Q2]
I understand VDIC is not supported YUV444, YUV422, and YUV400 even though these format are less than 8 bits/value, right?
Best Regards,
Satoshi Shimoda
Solved! Go to Solution.
Hi Satoshi
1. description below:
chapter 37.1.2.1.4.2 (DP), "Format: YUVA/RGBA, non-decimated, 8 bits/value"
cahpter 37.1.2.1.5.3 (IC), "Pixel format: YUV/RGB, 8 bits/value"
means that supported only these formats.
Regarding "less than 8 bits/value" - description also states:
"non-decimated", 8 bits/value - so not supported.
2. description below:
cahpter 37.1.2.1.5.3 (IC), "Pixel format: YUV/RGB, 8 bits/value"
means that YUV444 is supported. YUV420, YUV400 - not.
For YUV formats it may be suggested
to read YUV - Wikipedia, the free encyclopedia
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Satoshi
1. description below:
chapter 37.1.2.1.4.2 (DP), "Format: YUVA/RGBA, non-decimated, 8 bits/value"
cahpter 37.1.2.1.5.3 (IC), "Pixel format: YUV/RGB, 8 bits/value"
means that supported only these formats.
Regarding "less than 8 bits/value" - description also states:
"non-decimated", 8 bits/value - so not supported.
2. description below:
cahpter 37.1.2.1.5.3 (IC), "Pixel format: YUV/RGB, 8 bits/value"
means that YUV444 is supported. YUV420, YUV400 - not.
For YUV formats it may be suggested
to read YUV - Wikipedia, the free encyclopedia
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you for your reply, and sorry for my delay.
>1
OK, I understood that the supported format in DP and IC.
> 2
Would you let me know the supported format about VDIC also?
I have not understood well the following description.
"Pixel format: RGB/YUV 4:2:2, 8 bits/value"
RGB888 and YUV422 are supported even though YUV422 is not 8 bits/value?
Best Regards,
Satoshi Shimoda
Hi Satoshi
yes RGB888 and YUV422 are supported
Best regards
igor