i.MX6 CSI2IPU RGB444 and YUV422.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 CSI2IPU RGB444 and YUV422.

757 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SDL CSI2IPU.

Please see chapter 19.1.1 in IMX6DQRM, I want to confirm about " Dynamically configurable RGB444 and YUV422 data format for the IPU module".

I understand this is usable to adjust data alignment only when input data format is RGB444 or YUV422, so RGB444_FM bit and YUV422_8bit_FM bit in CSI2IPU_SW_RST register setting are "Dont' care" if other format is input.

Is my understanding correct?

Best Regards,

Satoshi Shimoda

Tags (1)
0 Kudos
1 Reply

421 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes this understanding is correct.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos