AnsweredAssumed Answered

Is it possible to create a updater.sb for the imx233 (stmp3780) that only has 8M sdram and no sdcard slot?

Question asked by j chaise on May 20, 2015
Latest reply on May 29, 2015 by j chaise

I have successfully initialized and tested the memory with the bootlets build via ltib, and loaded with the mfgtool.

When the kernel decompresses it will not fit in memory with the rootfs.

Should I start out with a already uncompressed kernel Image?

Is it possible to create a single ramdisk that has the kernel and the rootfs in it and load that into sdram?

This could be a read only rootfs right?

 

Should I invest time in yocto or stay with ltib?

I do not want to reinvent the wheel, just get a image flashed to the nand and spend my time developing it.

Outcomes