Hello
I'm using since a long time a system based on MC13213.
It is composed by an "End point" which send periodic data when a BP is pressed (else go to sleep and wakeup with KeyBoard interrupt)
And a coordinator which received data and make action accoding its. (Ack is sent to the end point)
So this system is very simple!
To do this, I started with the exemple MyWirelessAppDemoNonBeaconEndDevice & MyWirelessAppDemoNonBeaconCoordinator
Since last week, I update the system with the last beestack version 3.0.2: BeeKit HCS08 MAC Codebase 2.6.1
All is ok, but now, the "end point" also Wake up periodically (about 3 or 4 seconds)
It seems to me this is due to a functionnality which I don't remember if exist on my Old stack. This is called "indirect data": Data send by coordinator when end point is in sleeping..
I desactivate all managment of MLME in end point. But may be I forget something?
May be the problem come from other...
Then I don't find any way to desactivate a periodic wakeup. (I don't know at this time if it is the Transceiver or the µC timer which Wake up the µC
cPWR_DeepSleepMode is set to 1
Thank
Solved! Go to Solution.
Ok,
In fact, I think the µC wakeup because I seen courrent consumption pass from less than 1µA to 8 mA.
In fact, due to Serial link with a computer, current increase periodically I don't know why.
So the µC is keep in sleep.
Sorry:smileyblush:
Ok,
In fact, I think the µC wakeup because I seen courrent consumption pass from less than 1µA to 8 mA.
In fact, due to Serial link with a computer, current increase periodically I don't know why.
So the µC is keep in sleep.
Sorry:smileyblush: