I convert the CW10.6 example from C:\Freescale\CW MCU v10.6\MCU\CodeWarrior_Examples\Kinetis_Examples\k60
It pass the compiler, but fails on linker. The message is in the attached file.
Anyone can fix it?
Original Attachment has been moved to: KDS-Linker-Error-Message.txt.zip
Hello,
check your linker options of the project. You have something like this in it, probably starting with --start-group:
arm-none-eabi-gcc: error: unrecognized command line option '--undefined=__pformatter_'
arm-none-eabi-gcc: error: unrecognized command line option '--defsym=__pformatter=__pformatter_'
arm-none-eabi-gcc: error: unrecognized command line option '--start-group'
arm-none-eabi-gcc: error: unrecognized command line option '--end-group'
These are from the CW project, settings for the EWL libraries.
I hope this helps,
Erich