Good day guys!
I work with IMX287 and the latest version of LTIB from the site.
My question is about codecs as part fsl plugin. More specifically applies to the Speech codec type g723 g726 g729. Binary files are copied to /usr/lib and headers in /usr/include/imx-mm. I looked binaries libraries:
/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-fsl-linux-gnueabi-readelf -h rootfs/usr/lib/lib_g.723.1_dec_arm9_elinux.so
ELF Header:
Magic: 7f 45 4c 46 01 01 01 00 00 00 00 00 00 00 00 00
Class: ELF32
Data: 2's complement, little endian
Version: 1 (current)
OS/ABI: UNIX - System V
ABI Version: 0
Type: DYN (Shared object file)
Machine: ARM
Version: 0x1
Entry point address: 0x1614
Start of program headers: 52 (bytes into file)
Start of section headers: 68972 (bytes into file)
Flags: 0x4000002, has entry point, Version4 EABI
Size of this header: 52 (bytes)
Size of program headers: 32 (bytes)
Number of program headers: 5
Size of section headers: 40 (bytes)
Number of section headers: 31
Section header string table index: 28
Now compare with a working project:
/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-fsl-linux-gnueabi-readelf -h rootfs/usr/lib/libcpufreq.so
ELF Header:
Magic: 7f 45 4c 46 01 01 01 00 00 00 00 00 00 00 00 00
Class: ELF32
Data: 2's complement, little endian
Version: 1 (current)
OS/ABI: UNIX - System V
ABI Version: 0
Type: DYN (Shared object file)
Machine: ARM
Version: 0x1
Entry point address: 0x1328
Start of program headers: 52 (bytes into file)
Start of section headers: 12804 (bytes into file)
Flags: 0x5000002, has entry point, Version5 EABI
Size of this header: 52 (bytes)
Size of program headers: 32 (bytes)
Number of program headers: 6
Size of section headers: 40 (bytes)
Number of section headers: 27
Section header string table index: 24
Pay attention to the flags. Will work my projects with libraries of codecs?
The problem remained. In the composition of MM CODECS BUNDLE on the target platform have compiled examples:
root@freescale ls /usr/share/imx-mm/audio-codec/examples/g729/bin/
total 36
-rwxr-xr-x 1 root root 8538 Jun 5 09:30 test_g.729ab_dec_arm11_elinux
-rwxr-xr-x 1 root root 8494 Jun 5 09:30 test_g.729ab_dec_arm9_elinux
-rwxr-xr-x 1 root root 8763 Jun 5 09:30 test_g.729ab_enc_arm11_elinux
-rwxr-xr-x 1 root root 8687 Jun 5 09:30 test_g.729ab_enc_arm9_elinux
root@freescale /usr/share/imx-mm/audio-codec/examples/g729/bin$ ./test_g.729ab_enc_arm9_elinux /usr/share/test/test.wav ttt 0
BLN_MAD-MMCODECS_G729AB_ARM_03.01.00_ARM9 build on Mar 21 2012 17:09:44
Input speech file: /usr/share/test/test.wav
Output bitstream file: ttt
VAD disabled
Illegal instruction
root@freescale /usr/share/imx-mm/audio-codec/examples/g729/bin$
On the host:
mik@mik-VBox:~/PPP/ltib$ /opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-fsl-linux-gnueabi-readelf -h rootfs/usr/share/imx-mm/audio-codec/examples/g729/bin/test_g.729ab_enc_arm9_elinux
ELF Header:
Magic: 7f 45 4c 46 01 01 01 00 00 00 00 00 00 00 00 00
Class: ELF32
Data: 2's complement, little endian
Version: 1 (current)
OS/ABI: UNIX - System V
ABI Version: 0
Type: EXEC (Executable file)
Machine: ARM
Version: 0x1
Entry point address: 0x87e0
Start of program headers: 52 (bytes into file)
Start of section headers: 4996 (bytes into file)
Flags: 0x4000002, has entry point, Version4 EABI
Size of this header: 52 (bytes)
Size of program headers: 32 (bytes)
Number of program headers: 7
Size of section headers: 40 (bytes)
Number of section headers: 29
Section header string table index: 26
Hi,
As far as I understand the EABI should be backwards compatible. Therefore the it is expected a working functionality.
Best Regards,
Alejandro