AnsweredAssumed Answered

Android Kitkat imx6: How to use ABD over TCP by default

Question asked by Bill Butler on May 15, 2015
Latest reply on May 18, 2015 by Haoran Wang

On Mx6 Running kitkat android

 

Our design is not going to have the usb (otg) port available. I would like to set the adbd to use the tcp connections by default. I can get it to work but I have to restart adbd about reboot.

 

I have tried

 

root@nitrogen6x: # setprop persist.adb.tcp.port 5555

 

and added

 

system.adb.tcp.port=5555

 

/data/local.prop

    and/or

/system/build.prop

 

I can get adb to connect

         <sdk>\platform-tools> adb connect 172.16.0.45

 

ONLY if i restart adbd

 

root@nitrogen6x: # stop adbd

root@nitrogen6x: # start adbd

 

I don't under why this is required.. in system/core/adb/adb.c

 

I see

 

...

    // If one of these properties is set, also listen on that port

    // If one of the properties isn't set and we couldn't listen on usb,

    // listen on the default port.

    property_get("service.adb.tcp.port", value, "");

    if (!value[0]) {

        property_get("persist.adb.tcp.port", value, "");

    }

    if (sscanf(value, "%d", &port) == 1 && port > 0) {

        printf("using port=%d\n", port);

        // listen on TCP port specified by service.adb.tcp.port property

        local_init(port);

    } else if (!usb) {

        // listen on default port

        local_init(DEFAULT_ADB_LOCAL_TRANSPORT_PORT);

    }

 

I don't understand what is preventing it from starting correctly without adbd restart.

 

Any thoughts before I start ripping up the code :-)

Outcomes