Kernel Splash screen reg

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel Splash screen reg

636 Views
sachusanal
Contributor III

hello

I set a kernel splash screen in kernel image but it is loading so much late .I need to set splash screen in kernel which is loading at the time of kernel booting

please help me

Labels (1)
0 Kudos
1 Reply

399 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Have you tried with a smaller image? Have you verified the initialization order? You could refer to the following threads from the Community:

Re: delay between the boot loader and kernel splash screens

boot time optimisation reg(kernel side)

Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos