AnsweredAssumed Answered

Bitbake returns with error code while making image for imx6

Question asked by Ramprasad Vempati on May 13, 2015
Latest reply on May 17, 2015 by Ramprasad Vempati

I'm trying to make image "core-image-base" using bitbake for freescale imx6 platform. Things were working very well. I made image two times as well. But suddently it stopped working. I've used "bitbake core-image-base" command for making build.

 

below is the error I get. Could someone help me, what must have gone wrong?

'

| make: Leaving directory `/home/ramprasad/fsl-release-bsp-2/build-7/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.10.17-r0/image/usr/src/kernel'

| NOTE: make -j 4 imx6q-sabresd.dtb

|   CC      scripts/mod/devicetable-offsets.s

|   GEN     scripts/mod/devicetable-offsets.h

|   HOSTCC  scripts/mod/file2alias.o

|   HOSTLD  scripts/mod/modpost

| make[1]: `arch/arm/boot/dts/imx6q-sabresd.dtb' is up to date.

| NOTE: make -j 4 imx6q-sabresd-ldo.dtb

|   CC      scripts/mod/devicetable-offsets.s

|   GEN     scripts/mod/devicetable-offsets.h

|   HOSTCC  scripts/mod/file2alias.o

|   HOSTLD  scripts/mod/modpost

| make[1]: `arch/arm/boot/dts/imx6q-sabresd-ldo.dtb' is up to date.

| NOTE: make -j 4 imx6q-sabresd-hdcp.dtb

|   CC      scripts/mod/devicetable-offsets.s

|   GEN     scripts/mod/devicetable-offsets.h

|   HOSTCC  scripts/mod/file2alias.o

|   HOSTLD  scripts/mod/modpost

| make[1]: `arch/arm/boot/dts/imx6q-sabresd-hdcp.dtb' is up to date.

| NOTE: make -j 4 imx6q-sabresd-enetirq.dtb

|   CC      scripts/mod/devicetable-offsets.s

|   GEN     scripts/mod/devicetable-offsets.h

|   HOSTCC  scripts/mod/file2alias.o

|   HOSTLD  scripts/mod/modpost

    | make[1]: *** No rule to make target `arch/arm/boot/dts/imx6q-sabresd-  enetirq.dtb'.  Stop.

     make: *** [imx6q-sabresd-enetirq.dtb] Error 2

     ERROR: oe_runmake failed

     WARNING: exit code 1 from a shell command.

     ERROR: Function failed: do_install (log file is located at  /home/ramprasad/fsl-release-bsp-2/build-7/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.10.17-r0/temp/log.do_install.11111)

 

ERROR: Task 68 (/home/ramprasad/fsl-release-bsp-2/sources/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.10.17.bb, do_install) failed with exit code '1'

 

NOTE: Tasks Summary: Attempted 3610 tasks of which 3609 didn't need to be rerun and 1 failed.

No currently running tasks (1718 of 3640)

 

Summary: 1 task failed:

  /home/ramprasad/fsl-release-bsp-2/sources/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.10.17.bb, do_install

Summary: There was 1 ERROR message shown, returning a non-zero exit code

Outcomes