Dear Sir ,
i have mx6qsabresd board with me,when i flashing the image after the boot loader loading for the kernel booting so mant time is taken,and also i need to set a spalsh screen in kernel but the splash screen is loading after 6or 7 seconds, a blank screen is loading i need to avoid that blank screen also please help me to solve this issue
I here by attch my .config file for your reference.
Original Attachment has been moved to: .config.zip
Hi sachu
suggest to look at below link
Linux Fast Boot on i.MX6 Sabresd Board
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
In my kernel i set one splash screen but the splash screen is loading at last of the kernel section.
after the starting kernel print on terminal get along time to load splash screen what should i do