AN1931

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AN1931

581 Views
simon123
Contributor I

Hello,

 

Where can I finde the SW code due to app note AN1931 ?

 

Thanks

Labels (1)
0 Kudos
3 Replies

461 Views
trytohelp
NXP Employee
NXP Employee

Hi Simon,

Don't know if a software is associated to this AN.

I need to check it.

Keep you informed.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

461 Views
simon123
Contributor I

Hi Pascal,

Thanks a lot.

It will be great if you can find it.

I need the part of field weakening implementation for PMSM in the software code (i).

Thank you

0 Kudos

461 Views
trytohelp
NXP Employee
NXP Employee

Hi Simon,

I've received info from the Technical writer of this AN.

To resume...

This is a very old application based on 56F805 device.

The software was included in the SDK.

This example was build for old CodeWarrior development tool and not on last version.

There is a newer DRM102 including software too:

     http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDDSCPMSMVC&fasp=1

Other DRMs are available too (sensorless only).


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos