AnsweredAssumed Answered

Is it possible to use GStreamer SDK on iMX6? (CM-FX6)

Question asked by mad strum on May 12, 2015
Latest reply on May 26, 2015 by Bio_TICFSL

Hi,

 

I am recording video using the following pipeline.

 

gst-launch tvsrc fps-n=25 ! 'video/x-raw-yuv, width=(int)720, height=(int)576m framerate=(fraction)25/1' ! vpuenc codec=6 bitrate=1000000 ! avimux ! queue2 max-size-buffers=1 max-size-bytes=0 max-size-time=0 ! filesink location=output.avi

 

My question: Is it possible to use the GStreamer SDK on iMX6 platform on Debian armel (ARM) ? I don't see gst.h (basic requirement for gst SDK)  anywhere on my platform.

 

If yes, could somehow detail the steps to get it installed? I don't see it being supported on the GStreamer website installation portion. Installing on Linux - GStreamer SDK documentation - GStreamer SDK documentation

 

Many thanks.

Outcomes