Hi all,
My customer is using your AndroidBSP4.0(ICS) for their own board.
And they saw the reboot could fail during their repeated reboot test.
Because the following is written as ‘ known issue’ in the release note of Android4.0, they believe the issue is related to that.
“The loopback reboot tests may cause failure”
There is no similar description in the release note of AndroidBSP4.3.
Can I understand the known issue, the loopback reboot tests may cause failure, was solved in AndroidBSP4.3?
If so, can you provide the patch code for the AndroidBSP4.0 to solve the issue?
Thanks,
Miyamoto
Hi AVNET,
All the patch you can see are under the Updates and Patches (12) of i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale .
Here I recommend you to use the newest version BSP.
Hope this can help you.
Have a great day
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Dan,
Thanks for your comment.
Could you show me what patch can solve the reboot issue in R13.4-GA for Android 4.0.4?
And could you show me whether the reboot issue has been solved in the latest AndroidBSP?
Thanks,
Miyamoto