I'm porting bluez5 to the imx6 sabresd Development Board, of which Bluetoothctl need glibc_2.17.so, I cross compile glibc2.17, copy libc-2.17.so libc.so to the directory \lib of the file system, and download the image to Development Board,but freezes after turning on the Development Board, so how to upgrade glibc, I did anything wrong?do i need to recompile the file system?this is the error log:
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
devtmpfs: mounted
Freeing unused kernel memory: 272K (80beb000 - 80c2f000)
Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
CPU1: stopping
CPU: 1 PID: 26 Comm: kworker/1:1 Not tainted 3.10.17 #51
Workqueue: kinteractive_down cpufreq_interactive_freq_down
[<80013ae0>] (unwind_backtrace+0x0/0xf4) from [<80011504>] (show_stack+0x10/0x14)
[<80011504>] (show_stack+0x10/0x14) from [<80012d08>] (handle_IPI+0x108/0x118)
[<80012d08>] (handle_IPI+0x108/0x118) from [<80008584>] (gic_handle_irq+0x58/0x5c)
[<80008584>] (gic_handle_irq+0x58/0x5c) from [<8000dc80>] (__irq_svc+0x40/0x70)
Exception stack(0xab145d08 to 0xab145d50)