I am attempting to run a very basic build using imx-3.10.53-1.1.0_ga for the Freescale SABRE Smart Devices Platform.
I am following the instructions in the Freescale Yocto Project User's Guide, Document Number: IMXLXYOCTOUG, Rev L3.10.53_1.1.0-ga, 01/2015
The is the error:
| ERROR: Function failed: do_configure (log file is located at /media/flint/shd_ext4/freescale/imx-3.10.53-1.1.0_ga/build-x11/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/alsa-utils/1.0.27.2-r0/temp/log.do_configure.31027)
ERROR: Task 1567 (/media/flint/shd_ext4/freescale/imx-3.10.53-1.1.0_ga/sources/poky/meta/recipes-multimedia/alsa/alsa-utils_1.0.27.2.bb, do_configure) failed with exit code '1'
The error in the log file appears to be that panelw library is not found.
I believe that panelw is included in the ncurses package.
***LOG FILE IS ATTACHED TO THIS MESSAGE***
This is what I have done so far to try to fix the problem (among other things):
bitbake ncurses -c clean
bitbake alsa-utils -c clean
bitbake fsl-image-gui
And yet the error persists.
These are the commands I ran to set up the environment:
repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.53-1.1.0_ga
repo init
MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11 -e x11
bitbake fsl-image-gui
This is the build configuration that bitbake reports to me:
BB_VERSION = "1.22.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-14.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6qsabresd"
DISTRO = "poky"
DISTRO_VERSION = "1.6.2"
TUNE_FEATURES = "armv7a vfp neon callconvention-hard cortexa9"
TARGET_FPU = "vfp-neon"
Original Attachment has been moved to: log.do_configure.31027.zip