Hi, all
I want to use the signal PMIC_ON_REQ to trigger the external PMIC to power up the entire system. But now I encounter the problems. Firstly, when I turn off the system(via "adb reboot -p"), I measured the votage about the pin PMIC_ON_REQ is 2V, why? And when I pulg out the adapter, OK, no voltage, then pulg in the adapter, no voltage. But in the next time, only when my adapter was not plugged out (always connected) , shutdown the system,power up, over and over again, the pin PMIC_ON_REQ always is 2V. why? Refering to the manual reference, when system is turn on
Secondly,my settings are following, but when I turned off(via "adb reboot -p"), it didnt wake up. why? How to wake up?
cat /proc/driver/rtc
rtc_time : 00:09:20
rtc_date : 1970-01-02
alrm_time : 00:19:17
alrm_date : 1970-01-02
alarm_IRQ : yes
alrm_pending : no
update IRQ enabled : no
periodic IRQ enabled : no
periodic IRQ frequency : 1
max user IRQ frequency : 64
24hr : yes
alarm_IRQ : yes
Hi tony
this may be caused by overloading VDD_SNVS_IN voltage as described in
IMX6DQ6SDLHDG Table 2-6 Power and decouple recommendations
p.19. Please check also Chapter 8 Avoiding Board Bring-up Problems
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear igor,
And I find another problem, I write "1" to the bit PK_EN and PK_OVERRIDE, but I cant write value to the register,so the two problems are:
1. Why cant I write the value into the above register bits?
2. Could give me the info how to control the PMIC_ON_REQ with the above bits in detail?
3Q~