"Cannot open File", can someone help me?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"Cannot open File", can someone help me?

743 Views
Braulio_Cespede
Contributor III

I used beekit to create a Zigbee solucion.

but, this happend:

1.jpg

The problem is with a Lib, but I don't know how to solve it.

4 Replies

570 Views
Wilgaced
Contributor II

Dear Braulio and AngelC

the problem occurs when you select custom hardware, by example

in Beekit

* Select Target hardware "user defined configuration target"

* Edit custom target "MC13237C PiP"

so i think i could be eeprom config problem but not sure.

0 Kudos

570 Views
AngelC
Senior Contributor I

Dear Braulio,

Could you please specify the Codebase version and application template you are using? Also, please make sure you are using the latest BeeKit release 3.0.2 with updated solutions. Probably you are using an old version of it thus causing such problems.

Regards,

AngelC

0 Kudos

570 Views
Braulio_Cespede
Contributor III

Thanks for answer.

Beekit 3.0.2(Lastest update) Codebase 3.1.1 , Template Ha DimmableLight with MC13237.

Codewarrior 10.6 and CW 10.5 

0 Kudos

570 Views
AngelC
Senior Contributor I

Dear Braulio,

I just tested a new project using HCS08 BeeStack codebase 3.1.1 and the HA DimmableLight template without any issues at all. I exported the solution to CW10.6 and it compiled flawlessly. Could you please specify whether you selected the default options in Beekit’s project or you changed something else? Please also make sure you have a proper CW license or the evaluation version active.

Regards,

AngelC

0 Kudos